Hi all
My customer is evaluating the TIOS101 and they have below questions.
Please review and comment.
Best regards
Ueli
---------------------------------
9.2.2.3 Driving Inductive Loads
The datasheet states: This voltage is clamped internally at about 75 V.
Does this mean the voltage at the OUT pin can be > 50V ?
If we want to use a TVS diode: What voltage should we select ?
What happens if we drive an inductive load push-pull ? ...is demagnetization implemented ?
And do you have detailed functional description for operation with inductive loads (freewheeling) ?