Hi,
For TCAN1042HDR can pin 5 be connected to 5V via a resistor or must it be left disconnected compulsorily?
Thanks,
Antonio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For TCAN1042HDR can pin 5 be connected to 5V via a resistor or must it be left disconnected compulsorily?
Thanks,
Antonio
Hi Antonio,
Pin 5 for the non-'V' versions of TCAN1042 is a true internal no connect, meaning the state of this pin (within reason) will not impact device behavior. This allows compatibility with designs with footprints that implement other functions (such as split which is not needed with TCAN1042's driver). Connection to a 5V potential, with or without a resistor, is not a problem.
Regards,
Eric Schott