This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD3082E: connect with ISO7631F

Part Number: SN65HVD3082E
Other Parts Discussed in Thread: SN65HVD3083E, ISO7631FC

Dear Specialists,

My customer is considering SN65HVD3082E and ISO7631F and has a question.

I would be grateful if you could advise.

---

The R pin of the SN65HVD3083E is connected to the ISO7631FCDWR isolator_IN pin.

According to the ISO7631FCDWR data sheet, a constant current source, that is, a high resistance, is connected between the INC pin and GND.

The SN65HVD3083E data sheet P.18 Figure 25 shows an external pull-up (10 kohm) between the R pin and Vcc(+5V).

In this case, the voltage is divided with the high resistance inside the isolator, and the isolator input voltage drops.

So is it possible to make the external pull-up of the RS485 transceiver_R pin to a pull-down resistor?

ーーー

I appreciate your great help in advance.

Best regards,

Shinichi