Hi, there
Can I ask a question regarding the DS125DF111EVM: when 10Gbps Vpp=100mV data input was on channel B, everything works great, however when I just switch the input from channel B to channel A, no signal detected and current only 25 mA (3V).
I can not find any register would select each channel ? Is SMA1 and SMA5 can work both way as input/output as it is labled as "OutA+/InA+"?
Thanks alot
Regards
Jim