This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: About High-level and Low-level input voltage of XI pin

Guru 19610 points
Part Number: TUSB4020BI

Hi Team,

 

We would like to use external clock for XI pin.

I have two questions.

 

-------

[Q1]

We find High-level(VIH) and Low-level input voltage(VIL) of input pins but can’t find VIH and VIL of XI pin in the datasheet.

Could you please let us know VIH and VIL of XI pin?

 

[Q2]

If we use the external clock of following specification, does TUSB4020BIPHP work properly?

-High level=1.62V

-Low level=0.18V

 

<External Clock image>

 

-------

 

Regards,

Hide