Other Parts Discussed in Thread: TIC10024-Q1
Hi team,
When we see the VTH_COMP_3V, this spec says 2.85V - 3.3V is guaranteed for VS = 4.5 V to 35 V(test condition).
However VS_COMP says minimum Vs requirement for proper detection is 5.5V.
If we set the VTH_COMP=3V, Can TIC12400-Q1/TIC10024-Q1 operate properly at VS=4.5V which is minimum Recommended Operating Conditions?
If not what is the reason?
Thank you.
Regards,
Hirata