Hi,
Q1: UB927 whether or notcompatible deserializer of UB914/UB934/UB964;
Q2: the UB927 how to do configure Pattern mode;
Q3: the UB927 have received fpd-link signal, how to do configue register to work, and send to DES.
thank you.
xxz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Q1: UB927 whether or notcompatible deserializer of UB914/UB934/UB964;
Q2: the UB927 how to do configure Pattern mode;
Q3: the UB927 have received fpd-link signal, how to do configue register to work, and send to DES.
thank you.
xxz
Hello Xueze,
1) UB927 is not compatible with UB914/UB934/UB964. If you are looking for a compatible DES with parallel interface then you can use the UB926, and a DES with CSI-2 Interface then the UB940N is the right choice.
2) Please refer to this AppNote.
3) You do not need register configurations, you need to chose the correct Hardware configurations on Pins: BKWD, LFMODE, MAPSEL, REPEAT, IDx
HeXueze,
1) UB940 is not compatible with UB913/UB933.
2) Which device are you refering to? As I said, all the required steps and explanation are in the above mentioned AppNote.
3) Yes, the UB927 do supports 1280x720 @ 30FPS. The UB927 do support any PCLK from 5MHz to 85MHz.