Hello
We have a requirement to insert a voltage drop in a circuit that must withstand 1.5A (maximum and non-repetitive) for a few 10s of milliseconds. The data (SLVSED2C, Figure 2) shows the TVS0500 will clamp to 8 to 8.8V in this current range. So can the device replace a zener or am I overlooking something ?
Although the circuit is unlikely to reverse bias the device, I am interested to understand if the DC Forward Current limit of 500mA is the FET body diode and the damage if that is exceeded. Does the device become short or open circuit with that event ?
Harry