This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD3082E: the differential output current value when Vcc and Load changes.

Part Number: SN65HVD3082E

Dear Specialists,

My customer'd like to obtain a graph of the differential output current value when Vcc changes.

Data sheet P.8 Figure 6-5. Driver Differential Output Voltage versus Driver Output Current only describes Vcc = 5V.


They want a graph with the characteristics when Vcc = 5.5V and 4.5V.

The graphs of other company is shown for reference.( The other maker's product)

If possible, it would be nice if there was data when Vcc = 4V in addition.

They are investigating differential output current change and Vcc. 

I appreciate your great help in advance.

Best regards,

Shinichi