This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9539-Q1: how to use tca9539-Q1, just use read mode help

Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCA9539

Hi, anybody

I tested tca9539-Q1.

I read datasheet of tca9539. 

So, I understand the slave address this ic 0x74 / (A1, A0 is LOW, 1110100)

and to use it only read function, 0xE9 (1110100 '1')

I just use it only read function.

P0 port 0,1,2,3,4,5

p1 Port 17,16,15,14,13

I use microcontroller stm series, using HAL library.

i2C setting is fast mode, clock speed 400kHz.

First, I send start message to slave. 

HAL_I2C_Master_Transmit(&hi2c1, 0x74, data, 16, 10);

and than after 3ms delay
HAL_I2C_Master_Receive(&hi2c1, 0x74|0x01, data, 16, 10);

but, there is no reaction.

yellow is SDA, blue is SCL. I didin't know where is start signal, where is ack, SDA signal is really descrip 0x74? 

how can I do? 

thank you.