This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: The simulation model of TMUXHS4212

Part Number: TMUXHS4212

Hi sir,

It seems the simulation model supports only up to 0~15 GHz.

The S11 is over 0dB  after 15GHz, and that is unreasonable. 

However, we would like to do the simulation from 0 to 40GHz. 

Is there an official model to support 0~40GHz? or is there any other way to do that? Thanks!