This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DS90UB964-Q1: Does it compatible with 953 in 2MP camera application

Part Number: DS90UB964-Q1

HI team

I would like to ask that does our 964 compatible with 953 in 2MP pixel camera application? My colleagues asked you once and you reply was they could pair with each other under 1MP camera application. Besides, I see in 953 English version datasheet it said compatible with DS90UB964, is there a constraint for camera pixel requirement?

If 953 could compatible with 964, why does 964 only support 1MP camera in datasheet? Are there any constrains between 953-964? Since the 964 datasheet is old, do you have some schedule to update the 964 datasheet?   

  • Hello

        DS90UB953 can support 1MP, 60fps resolution and 2MP, 60fps resolution. 953 is certainly compatible with 964 as long as 953 is connected to a 1 MP 60fps Imager. If 953 is connected to a 2MP,60fps immager, then the output data rate of 953 will be much higher than what DS90UB964 can deal with. If the application is a 2MP,60fps resolution, then a DS90UB960 part needs to be used

    Thanks

    Vijay