Other Parts Discussed in Thread: TPS82084, , TMUX1309, BQ25300
I'm working on battery-powered device (headset/wireless mouse) with charging over USB.
Battery is quite large (2400 mAh for headset / 3400mAh for mouse) so current up to 1.8A will be used.
The device, however, needs to have USB data connection (to PC for audio transfer/settings/firmware updates), this is why most of the PD ICs won't suit.
This is also the reason I can't use more than 0.5A of current which is terribly low.
This is why I came up with an idea of using TUSB320 to know how much current is available and set charging current accordingly (0.5 A -> 0.5 A, 1.5 A -> 1.5A, 3A -> 1.8A).
Will this work for charging the device and using it at the same time?
Can you check that my schematic (this one is for headset) is correct and will do what I need? Please ignore things that are not related to power subsystem as it is unfinished.
Can you also recommend me IC for DC-DC buck conversion (1.8V+3.3V) which is cheap, easy to hand-solder and buy (so it will be available on Mouser/Digikey for order in about a month or less)? Now I'm using XCL209B series mainly because it has built-in inductor.