Hi,
Customer want to know more about the power up timing of the device.
Basically, they need to know what exactly mean by T5.5 and T5.8.
1. "Post power-up stabilization-time prior to MDC preamble for register access"
2. "PAM3 IDLE Stream from power-up (Master Mode)"
3.The impact if not following the power up timing requirement above (What will happen when not following the power up timing)
Customer have different understanding in the power timing requirement, can you confirm which is the correct one.
1. The 60ms is the max delay time from power stabilize to MDC preamble for register access. For example, if T5.5 = 200ms then it will be NOK.
2. The 60ms is the time needed for the DP83TC811R-Q1 to get ready before MDC preamble for register access. For example, if T5.5 = 200ms then it will be OK.
Thank you in advance.
Regards,
Maynard