Other Parts Discussed in Thread: TPD4E05U06-Q1, ESD122, TPD1E05U06
Hello folks,
I am thinking to use TPD4E02B04QDQARQ1 device to protect my PCB from ESD. As you know, TPD4E02B04QDQARQ1 is the passive ESD device and no need to power it.
In the datasheet, "The TPD4E02B04-Q1 supports signal ranges between –3.6 V and 3.6 V, which supports the SuperSpeed+ pairs on the USB Type-C application. " I wonder that can I use device for protect only DM and DP line? My type-c suppy voltage will 5 Volts but I think DM and DP lines cannot achive to 5 Volts. It should be lower, I dont know.
If it is not suitable for my design, could you evaluate TPD4E05U06-Q1?
By the way, This project is not BC1.2. Only passthrough from one connector to another.
Regards,
Mehmet.