Other Parts Discussed in Thread: ISO1500, ISO1410
Hello guys,
One of my customers is considering using SN65HVD3082E for their new products.
They have the following question about SN65HVD3082E. Could you please give me your reply for them?
Q1. I want to driver LED of a opt coupler with about 15mA as maximum by "R" output terminal of the device.
This 15mA is a pulse current not constant current. And the average current of LED driving will be less than 8mA of the recommended value.
Can "R" output terminal drive LED side of opt coupler with 15mA as maximum?
Q2. I think the average current of "R" output current must be less than +\-8mA.
Also I think the peak current (very small on duty) of "R" output current must be less than +\-24mA.
Is my understanding correct?
Your reply would be much appreciated.
Best regards,
Kazuya.