Other Parts Discussed in Thread: TCA9539,
Dear Expert,
I want to know when the TCA9539's I2C is disrupted, the GPIO will remain output level or reset to the power-on state?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Expert,
I want to know when the TCA9539's I2C is disrupted, the GPIO will remain output level or reset to the power-on state?
Thanks!
Haibin,
In the event of a time-out or improper operation, the system controller can reset the TCA9549-Q1 by asserting an active low input to the RESET input. This will put registers back to their default state setting I/O's to inputs and initializing the I2C-SMBus state machine.
Regards,
Tyler
Hi Tyler,
Yes, I know your mean. But I want to know is when the system controller was run abnormal lead to the I2C bus abnormal, what will be the I/O's state?
The output pins will change only at the ACK bit (that is, at the 27th or 36th clock edge) at the end of the register write (see figure 8-9).
A STOP condition will end the transaction. If the STOP condition is corrupted, the following clock cycles might be seen by the TCA9539-Q1 as the last part of the write transaction.