This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV001: DS90LV001 vs DS25BR100 / product longevity

Genius 17115 points
Part Number: DS90LV001

Hi all

My customer has a design where they have to connect two FPGAs via 2 lines at 300 Mbit. They like to use LVDS buffers and are looking at:

DS90LV001 800-Mbps LVDS buffer

DS25BR100 3.125-Gbps LVDS buffer with transmit pre-emphasis and receive equalization

SOP for this project is 2024 to remain in production till min. 2034, therefore they are concerned about the longevity / lifecycle of the above products.

Is one of the above a better choice regarding longevity ?

Or would you recommend another / more recent device ?

Best regards

Ueli