Other Parts Discussed in Thread: TIDA-01413, TPS65263, DS90UB960-Q1, DS90UB954-Q1, TPS650330, TEST
Hello team,
I discussed the issue of no link SER-DES below -30°C in recent time with Nick ...
Now we could isolate it: In Fail case there is a significantly increased oscillating of VDDPLL (pink curve - point 2; green - +1V8).
If we short circuit the ferrit bead at its ports the link establishes immediately and everthing is ok.
But it is a mystery to us, because this part of schematic has not been modified in our new design and layout.
Maybe an issue of the ferrit bead 742792662, but we couldn't confirm that.
The device selection seems to be ok and the bead has comparable features to the beads TI uses at its EVM kits.
By the way: In 953 data sheet there is a request for FB1-FB3: Z = 1 kOhm (@ 100 MHz) and RDC < 25 mOhm.
In several EVM kits the applied MURATA beads have up to 500mOhm RDC. Is the demand for <25mOhm to strong?
Regards,
Torsten