Other Parts Discussed in Thread: TCAN4550, ISO1044
Hi,I want to use CAN FD communicaiton with F28004X. Since the MCU doesn't have CAN FD hardware integrated in it.
So it seems that I have to use a CAN FD controller outside.
I think TCAN4550 is a choice, but what about TCAN114X series, is it can be used as a CAN FD transciever?
Since my application is for High voltage compressor controller in EV cars.
I have to do the isolation with CAN signal and MCU interface.
For TCAN4550, there are too much signals needed to be isolated.
Regards
Arrow