I tried interfacing my camera with DPHY440SSRHREVM, the input signal is 1.8V and the output signal i get is around 2.2 volts.
But I need MIPI signal in 1.8V only.
Is there anyway to configure it for 1.8V ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I tried interfacing my camera with DPHY440SSRHREVM, the input signal is 1.8V and the output signal i get is around 2.2 volts.
But I need MIPI signal in 1.8V only.
Is there anyway to configure it for 1.8V ?
Hi,
How are you connected to the DPHY440 EVM?
Is the 1.8V differential voltage? If it is, the 1.8V differential voltage is outside the DPHY440 Absolute Maximum Rating and can't be supported.
Thanks
David
Hi David (ASIC) Liu) ,
Sorry it was a typo mistake.
the input signal is 1.2V.
Is there any mipi configuration required for this EVM?
Hi,
The DPHY440 LP output max is 1.3V, so you shouldn't see 2.2V on the output.
You also need to make sure the source follows the MIPI spec. The DPHY440 retimer intends to boost the signal in HS mode only.
Thanks
David