Other Parts Discussed in Thread: DS90UB928QEVM
Dear TI Teams:
Now I am testing an onboard DS90UB925 with the Deserializer DS90UB928, below is the detailed information:
- Test equipment:
- DRA74X/DAR75X/TDA2X CPU Board
- DS90UB928QEVM
- Test condition
- HW
- Connect the two board with FPDLink Cable, this cable is ok when I test with 949 to 928
- DRA7xx EVM + 12V supply for the EVM
- 12V power supply for De-serializer board
- SW
- DS90UB925 just power on, no video signals appling on the pclk/hs/vs/de/vin[23:0] pins
- DS90UB928QEVM PDB keep high, LFMODE MAPSEL BISTEN OEN BISTC OSS_SEL all low, normal operation.
- HW
- RESULT
- DS90UB928QEVM pass signal keep high, but the lock signal always keep low.
- We can dump 925 reg list as below
- 0000: 36 00 00 d2 80 00 00 00 00 00 00 00 01 a0 00 00 6...............
0010: 00 00 00 1a 00 00 fe 5e a1 a5 00 00 00 00 00 00 .......^........
0020: 00 00 25 00 00 00 00 00 00 24 00 a0 00 00 00 00 ..%......$......
0030: 03 10 00 00 00 00 08 34 00 0a 20 21 00 00 f0 00 .......4.. !....
0040: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
0050: 2f 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 /...............
0060: 00 00 00 00 10 00 00 00 00 00 00 00 00 00 00 00 ................
0070: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
0080: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
0090: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00c0: 00 00 80 00 48 08 00 00 40 00 00 00 00 00 00 00 ....H...@.......
00d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00f0: 5f 55 42 39 32 35 00 00 00 00 00 00 00 00 00 _UB925......... - You can see just link on reg 0xc[0], no DES ID on reg 0x6
- Futher try
- I set ds90ub925 to generate a pattern use internal clock, no effect. The reg setting is shown below
- 0x66 0x03
0x67 0x06
0x66 0x07
0x67 0x20
0x66 0x08
0x67 0x03
0x66 0x09
0x67 0x1e
0x66 0x04
0x67 0x98
0x66 0x05
0x67 0xd4
0x66 0x06
0x67 0x20
0x66 0x0c
0x67 0xd8
0x66 0x0d
0x67 0x23
0x66 0x0a
0x67 0x0a
0x66 0x0b
0x67 0x02
0x66 0x0e
0x67 0x03
0x66 0x03
0x67 0x11
- Questions
- Why ds90ub928 can lock? This board can lock when testing with ds90ub949 evm board.
- If I should apply signals on the pclk/hs/vs/de/vin[23:0] pins? If so, how can I let 928 locked with these signals absenting?
- If the pattern I used for 925 ok or not?
- What is the lock mechanism between Deserializers and Serializers? That is to say, what is the condition of locking?
- If there are error configurations if ds90ub925?
Hope you can see this and help me asps.
Thank you very much for taking the time out of your busy schedule to help me answer these!