Part Number: TCA9536
Dear Experts,
For the following virtual situation, I would like to confirm two items.
# 1. VCC Input 1.8V, SDA and SCL are pulled up to 3.3V. In my understanding, TCA9536 is acceptable in this situation. Is it correct?
# 2. The P0 output goes low. Then the voltage of P0 line will be under the 0.013V (Almost GND). Is it correct?

I would appreciate it if you could answer it.
Regards