Hi
I would like to ask you some questions as below.
Though my customer has been trying to use PRBS function, they have failed to get output PN pattern signal yet.
They set the register setting by "SNLU182B 6.22".
Q1) About the output bit rate of PRBS pattern, the rate is fixed to the specific rate?
Q2) The setting sequence of the customer is following. Is this correct?
add data
---------------
2Eh 04h
30h 01h
1Eh 10h
79h 00h
79h 20h
30h 00h
30h 08h
1Eh 80h
09h 20h
Thank you for your support.
Best Regards,