This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949A-Q1: lose remote control of DS90UB948

Part Number: DS90UB949A-Q1


Hi,

    1.Our HW setup is : DS90UB949A----(2-lane twisted STP)-----DS90ub948----(dual-link LVDS)-----TFT LCD(1920x720)

    2.Experiment results:

       (1)LCD can show normal test pattern(1920x720 @ 60fps) after initiated DS90UB949A, and remote control on DS90UB948 works fine.

       (2)When host processor output HDMI source to DS90UB949A with a TMDS freq of 90MHz(read from REG[0x5F]), remote control works fine.

       (3)When host processor output HDMI source to DS90UB949A with a TMDS freq of 118.8MHz(read from REG[0x5F]),lose remote control on DS90UB948

       (4)check REG[0x5A] of DS90UB949A is 0xCD, REG[0x1C] of DS90UB948 is 0x3B. It seems dual-link FPD-link is correct.

Question:

      (1)Does TMDS freq above 105MHz cause this issue? In dual-link FPD-LINK mode, maximum value of REG[0x5F] is 210MHz?

      (2)Any other items we need check against?