こんにちは
私はTMUXHS4212が差動ICであることを理解しています。
しかし、N側を50オームで終端させることができ、P側のみを単独で使用できますか?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
こんにちは
私はTMUXHS4212が差動ICであることを理解しています。
しかし、N側を50オームで終端させることができ、P側のみを単独で使用できますか?
If you use P, just leave N floating, don't terminate.
Regards
Brian
Thank you for answering.N is floating NG I understand.
Is the following usage OK?
P is signal,N is 50ohm termination.
if N is 50 ohm terminated, need to terminated on both side of the mux.
Regards
brian