Hi,
How to read s erializer UB913 regiter status through Deserializer ub964, I want to configure the UB913 regiter.
Thank you.
Best Regards,
xueze.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
How to read s erializer UB913 regiter status through Deserializer ub964, I want to configure the UB913 regiter.
Thank you.
Best Regards,
xueze.
搜索
复制
Hi Xueze,
The first step is to make sure that the UB964 and UB913 devices are all LOCKed to each other. If the MODE settings on the deserializer & serializers match and there are no issues with the PCB or cable, then they should LOCK.
To setup slave addresses for the connected serializers, refer to the following steps in the UB964:
Best,
Justin Phan