This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV001: Could this DS90LV001 used for drive MIPI-DSI in video mode through cable to MIPI-DSI LCD

Part Number: DS90LV001

Hi,

Could it be possible to use this kind of LVDS driver to buffer our MPUs 2 lane + clock MIPI-DSI interface through 5-6m cable to external MIPI display?

I have understood that MIPI displays can also operate in video mode and with unidirectional interface. Maybe question is that do you have LVDS buffers which can drive ~600MHz signals through 5-6 meter USB-C cable and of course in MIPI-DSI interface jitter specification? Our LCD would be 1280x800 resolution with 16-24bit colors