Hi team,
There are two questions about SN75LVPE802
1. What level of DEW2 (pin 6) is recommended to be set when using transfer rate of 3Gbps by SATA? If set to low, what will be the effect on signal function and quality?
2. Is there an internal pull-up in the pin DEW2 (pin 6)? It is not clearly stated in the datasheet.
Thanks a lot,
Matthew Chen