This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LBC179: How to meet IEC 61000-4-2 standards

Part Number: SN65LBC179
Other Parts Discussed in Thread: THVD1551, , TPD2E007

Hello,

I have a customer who is looking to use the SN65LBC179Q but needs their solution to meet IEC 61000-4-2 standards. Do you have a recommendation for additional circuitry/parts to pair with the SN65LBC179Q to accomplish this?

If there is an alternative TI device which meets IEC 61000-4-2 standards, and is readily available, we are open to that as well. We found the THVD1551 as being one option here but it is sold out everywhere so this may not be a suitable short-term option.

Best regards,

Matt Calvo