Hi Team,
I don't see this spec in datasheet. How to know a protector IC pin maximum withstand voltage? If input maximum voltage is about 60V, can it limit pin voltage to about 30V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I don't see this spec in datasheet. How to know a protector IC pin maximum withstand voltage? If input maximum voltage is about 60V, can it limit pin voltage to about 30V?
Hi Dillen,
Are you referring to the maximum normal operating voltage? If so, the is the diode's Vrwm would be the spec you need to look at. For example, if you are wanting to protect an I/O line who's signal operates between 0 and 5 V, you would need a diode with a Vrwm of at least 5 V.
If you're referring to the max voltage the IC being protected can withstand during a surge or ESD event, you will need to refer to the clamping voltage of the diode to see what can effectively protect your IC: https://e2e.ti.com/blogs_/b/powerhouse/posts/esd-fundamentals-part-3-clamping-voltage
Regards,
Matt Smith