Other Parts Discussed in Thread: TPS65987D, TPS55288, LM3489, LM5175, PMP20042, LM61460, LM61440
hi TI
The customer needs to make the source end, battery powered, 24V input, and 100W output power to charge the mobile phone. There is no data communication demand. Is there a chip that meets the wide temperature(-40 ℃ ~85 ℃) version and can be provided according to the overall design scheme?
I found only 6 chips meeting 100W power, all of which are -10~75 ℃。