Part Number: TPS65988EVM
Hi TI,
I connect one end of the type-c cable plug to PortA, and the other end plug to the device, then read the 0x49 register to get the SOP' data, the VDM version of the data is 1.0.
Some connected devices can read SOP' data with VDM version 2.0 by using the "VDMs" command, but some devices cannot.
What can I do so that the "VDMS" command works when any device is connected?
Or is it possible to read SOP' (VDM version 2.0) from the beginning without using the "VDMs" command?
Thanks
Wilson