Hi Team,
My customer is considering TUSB8041IPAPQ1 and he wants to use 3 ports for USB3.0 and 1 port for USB2.0.
Customer have following questions, could you kindly help?
1. Can TUSB8041IPAPQ1 be used for USB3.0 and USB2.0 together?
2. When using USB2.0, following pins is unused. From following material, it says just leave it unconnected and no terminal is needed if downstream port is not connected. Is this also the same when using USB2.0?
https://www.ti.com/lit/an/slla410/slla410.pdf
・USB_SSRXP_DN*
・USB_SSRXM_DN*
・USB_SSTXP_DN*
・USB_SSTXM_DN*
3. Is there anything customer should care about when using USB3.0 and USB2.0 together? It will be great if there's any material.
Thanks.
Regards,
Jo