This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDES960: I2C programming requirements

Part Number: TDES960

Hello,

I'm trying to programm TDES960 I2C register from  I2C_SCL pin12 and I2C_SDA pin11 pulled by 3.7K to VCC (3.3V).

The PDB pin is pulled to 3.3V by 10K with 10µF capacitor as suggest in 9.2.1.

My problem is I cannot obtain Acknowledge from I2C 7bit address 0x3D B0111101 . VIDX pulled to 1V8.

Is there something else to verify to know if the I2C bus is operational?

Thank you.

Regards.