Other Parts Discussed in Thread: TIC12400
Hello experts
We used TI's TIC12400 chip. After it was loaded and used for a period of time, a fault occurred. The switch status collected by the 12400 chip could not follow the change.
With the debugger, all the switches collected by the TIC12400 chip are 0 (that is, all the values given to the upper layer are 1 after inverting).
After the debugger is installed, the ID of device 12400 read is 0, and all values in the status register are 0. According to the driver design logic, ECU running process, if the chip failure, will lead to periodic reset. -- After several tests, it is found that the chip is reset "repeatedly", and each reset fails (that is, the chip driver initialization is unsuccessful).
Attached is the schematic diagram.