This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3232E: TRS3223 voltage rating question

Part Number: TRS3232E

Hi,

According to the spec, The output driver range is -13.2~13.3V,

I want to know what voltage are acceptable if there are back power from another side?

-13.2~13.3V?

or -25~25V are acceptable, (Same as input voltage range)

thank you.