Hi Support Team.
Please tell me the following information of XIO2001IZAJ.
・Copper pad diameter(mm)
・Copper pad thickness(mm)
・Solder mask openting diameter(mm)
・Solder mask openting thickness(mm)
↓Reference diagram
Thanks,
Yutaro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support Team.
Please tell me the following information of XIO2001IZAJ.
・Copper pad diameter(mm)
・Copper pad thickness(mm)
・Solder mask openting diameter(mm)
・Solder mask openting thickness(mm)
↓Reference diagram
Thanks,
Yutaro
Hi Yutaro-san,
Most of the ZAJ package information is available here: ZAJ (S-PBGA-N144) 4207337-2 (Rev. A) (ti.com)
The measurements you are asking for are not listed, so I will need to ask internally to see who might have the answer. Please allow me some time to do this.
Regards,
Nicholaus
Hi Nicholaus
sorry.
The requested model name was DS160PT801ACBR, not XIO2001IZAJ.
It's my typing error.
I would like information on the DS160PT801ACBR.
Yutaro
Hi Yutaro,
Alright thanks. I have asked the internal team and am waiting for a response.
Regards,
Nicholaus
Hi Yutaro,
I have received a response about the DS160PT801ACBR.
Note, there are 2step SR on Die mount side of substrate.
SR thickness beneath the die is 15um.
SR thickness on the rest of area is 25um.
Regards,
Nicholaus