Part Number: TL16C552
Hello: We are planning on using TL16C552FN or TL16C552AFN but have several questions:
1.) Is there an option for TL16C552IFN? (We want to use TL16C552FN as a drop in for ST16C552IJ68 but would like an industrial rating)
2.) The TI spec calls out -40 to 85C for TL16C552AFN. Shouldn't it be 0 to 70C? Should TL16C552AIFN be -40 to 85? (Due to the -I suffix)

3.) The power rating for TL16C552AFN is 865mW @70C derated 19mW/C after 25C. Is my understanding correct in that it calculates to around 577mW at 85C?
Regarding TL16C552FN, it is rated at 500mW @70C. Why are these different, or are they the same but the spec was written differently? What is the derating for TL16C552FN? Additionally, would be the derating for
TL16C552IFN if that part is available?
4.) Would these power ratings change depending on how fast you were clocking the part? For instance, we use the TL16C552FN @ 1.843 MHz so should we expect a quarter of the max amp draw given its max frequency is 8 MHz?
5.) Regarding Tjamx, RthetaJA, and RthetaJC, are these values the same for both TL16C552AFN and TL16C552FN?
6.) TL16C552FN has 4 levels of prioritization for interrupts. Does TL16C552AFN have the same?
7.) The RESET line for TL16C552FN is specified to be low for 1uS after Power Up. Is TL16C552AFN the same?
8.) The RESET conditions between the parts are the same with exception that the interrupt lines are cleared for TL16C552FN but are low for TL16C552AFN. Is this a spec wording issue or are they different?