Hello Team,
Posting on behalf of customer:
I have a project which requires me to send a data and clock signal which uses SPI protocol over a large distance. As I will be using a high frequency above 100mhz, I want to use differential signalling to reduce EMI. So, will I be able to use the DS90LV047A to distribute a clock signal over a differential signal pair?
I need to send a unidirectional clock and data signal over a large distance at a frequency over 100mhz. I want to know if the DS90LV047A is suitable to input into this component and if it will output two differential pairs, for both the data AND clock. Or if I should use a different component for this application.
Regards,
Renan