This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826EVM: A Layout Question of surge voltage protection on RJ45 Differential Pair Routing

Part Number: DP83826EVM

Dear TI Expert,

  We have a quite detailed layout quesiton which concerns us on the aspect of EMC surge test. In the pcb design file of DP83826EVM, we can see the routing of signal trace on the top layer and PGND copper pour on the second layer for RJ45 section, as below:

Top Layer

                  

Second or Other Layer

The through mount RJ45 connector would make differential signal quite close to second and other layer PGND via the through hole, as shown in the screenshot.

If there's a high surge voltage, say 1 or 2kV for EMC surge test coupling into the ethernet cable, the spacing or clearance seems not enough, which may break down and damage the clearance and make signal line conduct to PGND for good.

Correct me if I am wrong, e.g. according to IPC-2221, the clearance calulated for 1kV (DC or AC) should be 1.5mm or so for internal layer, which is far larger than the spacing as we see now. 

How should we consider this? Do we miss or misunderstand anything? Would appreciate any advice or suggestion.

Regards,

Yuanchen Zhu