Hi team,
I have some question regarding TCAN1463-Q1 Pin usage.
Could you give comments for below?
1. INH
Is it used for toggle enable (power by DCDC) when device wakes up from sleep by CAN input?
2. Wake
2-1. It seems that it is uses when there's external wake up switch. What's the connection when there's no switch? Connect directly to Vbat?
2-2. What should I do with WAKE pin when there's no need of LWU and only to wake device by CAN signal? NC?
3. INH-Mask
What's the purpose of the pin?
5. nSTB
Does it receive input signal by MCU to identify device is in STB status?