This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PT801X16EVM: DS160PT801X16EVM

Part Number: DS160PT801X16EVM

I can't see proper retimer(DS160PT801X16EVM) Gen3 performance with NVMe.
Please check my test results and then give me feedback. 

1. Test Environment
1) ubuntu PC : Intel(R) Core(TM) i9-10900 CPU, 64GB Memory PC
2) ubuntu Version : Ubuntu 18.04.6 LTS
3) Retimer : DS160PT801X16EVM
4) NVMe : Micron MVMe Gen3 x4. 21100AT M.2 SSD

2. My Three Test Cases
1) Direct NVMe connection through PCIe Slot : Main board <-> PCIe to M.2 convert board <-> NVMe
   NVMe is normally recognized as PCIe Gen3(ASPM Disabled) and Good Stable performance

2) Use TI Retimer : Main board <-> TI retimer(DS160PT801X16EVM) <-> PCIe to M.2 convert board <-> NVMe
   NVMe is normally recognized as PCIe Gen3(ASPM L1 Enabled) and But Unstable performance

3) Use TI Retimer(Force Gen2 in BIOS Setting) : Main board <-> TI retimer(DS160PT801X16EVM) <-> PCIe to M.2 convert board <-> NVMe
   NVMe is recognized as PCIe Gen2 and Stable performance

3. Detail Test Result
1) Direct NVMe connection through PCIe Slot
1-1) lspci -vv
01:00.0 Non-Volatile memory controller: Micron Technology Inc Device 6001 (rev 03) (prog-if 02 [NVM Express])
Subsystem: Micron Technology Inc Device 2100
Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Latency: 0, Cache Line Size: 64 bytes
Interrupt: pin A routed to IRQ 16
NUMA node: 0
Region 0: Memory at b1300000 (64-bit, non-prefetchable) [size=16K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [50] MSI: Enable- Count=1/8 Maskable+ 64bit+
Address: 0000000000000000 Data: 0000
Masking: 00000000 Pending: 00000000
Capabilities: [70] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 128 bytes, PhantFunc 0, Latency L0s unlimited, L1 unlimited
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset+ SlotPowerLimit 25.000W
DevCtl: Report errors: Correctable+ Non-Fatal+ Fatal+ Unsupported+
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop- FLReset-
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr+ TransPend-
LnkCap: Port #0, Speed 8GT/s, Width x4, ASPM L1, Exit Latency L0s <1us, L1 <8us
ClockPM+ Surprise- LLActRep- BwNot- ASPMOptComp+
LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk+
ExtSynch- ClockPM+ AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 8GT/s, Width x4, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, LTR+, OBFF Not Supported
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR+, OBFF Disabled
LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete+, EqualizationPhase1+
EqualizationPhase2+, EqualizationPhase3+, LinkEqualizationRequest-
Capabilities: [b0] MSI-X: Enable+ Count=16 Masked-
Vector table: BAR=0 offset=00002000
PBA: BAR=0 offset=00002100
Capabilities: [100 v2] Advanced Error Reporting
UESta: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UEMsk: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
CESta: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
CEMsk: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
AERCap: First Error Pointer: 00, GenCap+ CGenEn- ChkCap+ ChkEn-
Capabilities: [158 v1] #19
Capabilities: [178 v1] Latency Tolerance Reporting
Max snoop latency: 3145728ns
Max no snoop latency: 3145728ns
Capabilities: [180 v1] L1 PM Substates
L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
PortCommonModeRestoreTime=10us PortTPowerOnTime=10us
L1SubCtl1: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+
T_CommonMode=0us LTR1.2_Threshold=81920ns
L1SubCtl2: T_PwrOn=44us
Kernel driver in use: nvme
Kernel modules: nvme

1-2) iozone : 
Iozone: Performance Test of File I/O
Version $Revision: 3.429 $
Compiled for 64 bit mode.
Build: linux-AMD64

Contributors:William Norcott, Don Capps, Isom Crawford, Kirby Collins
Al Slater, Scott Rhine, Mike Wisner, Ken Goss
Steve Landherr, Brad Smith, Mark Kelly, Dr. Alain CYR,
Randy Dunlap, Mark Montague, Dan Million, Gavin Brebner,
Jean-Marc Zucconi, Jeff Blomberg, Benny Halevy, Dave Boone,
Erik Habbinga, Kris Strecker, Walter Wong, Joshua Root,
Fabrice Bacchella, Zhenghua Xue, Qin Li, Darren Sawyer,
Vangel Bojaxhi, Ben England, Vikentsi Lapa.

Run began: Wed Jan 11 11:00:33 2023

Record Size 4 kB
Record Size 8 kB
Record Size 64 kB
Record Size 256 kB
Record Size 512 kB
Record Size 1024 kB
Record Size 2048 kB
Record Size 4096 kB
SYNC Mode.
O_DIRECT feature enabled
File size set to 10240 kB
Command line used: iozone -r 4k -r 8k -r 64k -r 256k -r 512k -r 1024k -r 2048k -r 4096k -o -I -s 10m -f /mnt/nvme/iozone
Output is in kBytes/sec
Time Resolution = 0.000001 seconds.
Processor cache size set to 1024 kBytes.
Processor cache line size set to 32 bytes.
File stride size set to 17 * record size.
random random bkwd record stride
kB reclen write rewrite read reread read write read rewrite read fwrite frewrite fread freread
10240 4 1224 1152 150872 150758 50474 3292 50177 1069 69121 3931030 5601299 9276776 8145506
10240 8 1611 1801 286947 287262 92531 1667 92974 1691 119388 4338874 6161364 11058656 9454437
10240 64 11307 11714 1240753 1253975 314495 19624 221161 14766 224334 4679732 7247904 14143042 11326970
10240 256 27352 35061 1438377 1422183 699645 25980 548150 37518 513151 4473548 6191563 12996126 11010462
10240 512 85987 67706 1542632 1519492 1066998 103170 826403 69746 1035285 4555155 6568427 13528283 10987927
10240 1024 102181 128907 1487084 1596238 999601 104402 1262935 131351 1002845 4477746 6456844 19849135 10882135
10240 2048 415974 387482 1639187 1605006 1129012 387776 1057748 471498 1064011 3932469 6525515 12381688 10468366
10240 4096 635575 569919 1611634 1699563 1168308 903186 1115329 996835 1121298 4763052 10463389 15279105 13744963

iozone test complete.

1-3) hdparm : while true; do sudo hdparm -t /dev/nvme0n1; sleep 1; done
/dev/nvme0n1:
Timing buffered disk reads: 5572 MB in 3.00 seconds = 1857.12 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5566 MB in 3.00 seconds = 1854.96 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5558 MB in 3.00 seconds = 1851.99 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5576 MB in 3.00 seconds = 1858.14 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5556 MB in 3.00 seconds = 1851.91 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5460 MB in 3.00 seconds = 1819.75 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5550 MB in 3.00 seconds = 1849.63 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5550 MB in 3.00 seconds = 1849.37 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5522 MB in 3.00 seconds = 1840.40 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5474 MB in 3.00 seconds = 1824.22 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5330 MB in 3.00 seconds = 1776.39 MB/sec

2) Use TI Retimer
2-1) lspci -vv
01:00.0 Non-Volatile memory controller: Micron Technology Inc Device 6001 (rev 03) (prog-if 02 [NVM Express])
Subsystem: Micron Technology Inc Device 2100
Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Latency: 0, Cache Line Size: 64 bytes
Interrupt: pin A routed to IRQ 16
NUMA node: 0
Region 0: Memory at b1300000 (64-bit, non-prefetchable) [size=16K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [50] MSI: Enable- Count=1/8 Maskable+ 64bit+
Address: 0000000000000000 Data: 0000
Masking: 00000000 Pending: 00000000
Capabilities: [70] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 128 bytes, PhantFunc 0, Latency L0s unlimited, L1 unlimited
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset+ SlotPowerLimit 75.000W
DevCtl: Report errors: Correctable+ Non-Fatal+ Fatal+ Unsupported+
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop- FLReset-
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr+ UncorrErr- FatalErr- UnsuppReq- AuxPwr+ TransPend-
LnkCap: Port #0, Speed 8GT/s, Width x4, ASPM L1, Exit Latency L0s <1us, L1 <8us
ClockPM+ Surprise- LLActRep- BwNot- ASPMOptComp+
LnkCtl: ASPM L1 Enabled; RCB 64 bytes Disabled- CommClk+
ExtSynch- ClockPM+ AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 8GT/s, Width x4, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, LTR+, OBFF Not Supported
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR+, OBFF Disabled
LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete+, EqualizationPhase1+
EqualizationPhase2+, EqualizationPhase3+, LinkEqualizationRequest-
Capabilities: [b0] MSI-X: Enable+ Count=16 Masked-
Vector table: BAR=0 offset=00002000
PBA: BAR=0 offset=00002100
Capabilities: [100 v2] Advanced Error Reporting
UESta: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UEMsk: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
CESta: RxErr+ BadTLP- BadDLLP+ Rollover- Timeout- NonFatalErr-
CEMsk: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
AERCap: First Error Pointer: 00, GenCap+ CGenEn- ChkCap+ ChkEn-
Capabilities: [158 v1] #19
Capabilities: [178 v1] Latency Tolerance Reporting
Max snoop latency: 71680ns
Max no snoop latency: 71680ns
Capabilities: [180 v1] L1 PM Substates
L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
PortCommonModeRestoreTime=10us PortTPowerOnTime=10us
L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
T_CommonMode=0us LTR1.2_Threshold=0ns
L1SubCtl2: T_PwrOn=10us
Kernel driver in use: nvme
Kernel modules: nvme

2-2) iozone
Iozone: Performance Test of File I/O
Version $Revision: 3.429 $
Compiled for 64 bit mode.
Build: linux-AMD64

Contributors:William Norcott, Don Capps, Isom Crawford, Kirby Collins
Al Slater, Scott Rhine, Mike Wisner, Ken Goss
Steve Landherr, Brad Smith, Mark Kelly, Dr. Alain CYR,
Randy Dunlap, Mark Montague, Dan Million, Gavin Brebner,
Jean-Marc Zucconi, Jeff Blomberg, Benny Halevy, Dave Boone,
Erik Habbinga, Kris Strecker, Walter Wong, Joshua Root,
Fabrice Bacchella, Zhenghua Xue, Qin Li, Darren Sawyer,
Vangel Bojaxhi, Ben England, Vikentsi Lapa.

Run began: Thu Jan 12 11:33:14 2023

Record Size 4 kB
Record Size 8 kB
Record Size 64 kB
Record Size 256 kB
Record Size 512 kB
Record Size 1024 kB
Record Size 2048 kB
Record Size 4096 kB
SYNC Mode.
O_DIRECT feature enabled
File size set to 10240 kB
Command line used: iozone -r 4k -r 8k -r 64k -r 256k -r 512k -r 1024k -r 2048k -r 4096k -o -I -s 10m -f /mnt/nvme/iozone
Output is in kBytes/sec
Time Resolution = 0.000001 seconds.
Processor cache size set to 1024 kBytes.
Processor cache line size set to 32 bytes.
File stride size set to 17 * record size.
random random bkwd record stride
kB reclen write rewrite read reread read write read rewrite read fwrite frewrite fread freread
10240 4 190 189 1485 1476 668 189 670 190 664 3868362 5599108 9191409 8178077
10240 8 381 382 2891 2879 1316 379 1330 381 1326 4366665 6360270 11084342 9652033
10240 64 2821 2800 11338 12033 10698 2733 9529 2821 9710 4541187 6653906 13232361 10976694
10240 256 8776 9138 17760 18405 17027 8717 16369 9210 16234 4406538 6313523 12753013 10732573
10240 512 13013 14783 21977 21190 20961 14627 20615 12951 21420 4376008 6320956 12753013 10676546
10240 1024 21096 18209 22918 24149 21757 17426 22099 18181 24217 4524921 6058802 12518829 10524802
10240 2048 24343 26197 27604 25682 27095 22776 23909 23054 25857 3694021 5550626 12119646 10273061
10240 4096 30685 29030 24863 28628 26523 22640 26789 31673 24196 4149824 7802283 10460204 9224572

iozone test complete.

2-3) hdparm
/dev/nvme0n1:
Timing buffered disk reads: 5584 MB in 3.00 seconds = 1861.24 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 92 MB in 3.04 seconds = 30.29 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 88 MB in 3.04 seconds = 28.97 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 122 MB in 3.06 seconds = 39.92 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5556 MB in 3.00 seconds = 1851.95 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5588 MB in 3.00 seconds = 1862.45 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 76 MB in 3.05 seconds = 24.90 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 154 MB in 3.03 seconds = 50.78 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 74 MB in 3.02 seconds = 24.54 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 142 MB in 3.03 seconds = 46.81 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 5550 MB in 3.00 seconds = 1849.89 MB/sec

3) Use TI Retimer(Force Gen2 in BIOS Setting)
3-1) lspci -vv
01:00.0 Non-Volatile memory controller: Micron Technology Inc Device 6001 (rev 03) (prog-if 02 [NVM Express])
Subsystem: Micron Technology Inc Device 2100
Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Latency: 0, Cache Line Size: 64 bytes
Interrupt: pin A routed to IRQ 16
NUMA node: 0
Region 0: Memory at b1300000 (64-bit, non-prefetchable) [size=16K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [50] MSI: Enable- Count=1/8 Maskable+ 64bit+
Address: 0000000000000000 Data: 0000
Masking: 00000000 Pending: 00000000
Capabilities: [70] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 128 bytes, PhantFunc 0, Latency L0s unlimited, L1 unlimited
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset+ SlotPowerLimit 75.000W
DevCtl: Report errors: Correctable+ Non-Fatal+ Fatal+ Unsupported+
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop- FLReset-
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr+ TransPend-
LnkCap: Port #0, Speed 8GT/s, Width x4, ASPM L1, Exit Latency L0s <1us, L1 <8us
ClockPM+ Surprise- LLActRep- BwNot- ASPMOptComp+
LnkCtl: ASPM L1 Enabled; RCB 64 bytes Disabled- CommClk+
ExtSynch- ClockPM+ AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 5GT/s, Width x4, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, LTR+, OBFF Not Supported
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR+, OBFF Disabled
LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete-, EqualizationPhase1-
EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
Capabilities: [b0] MSI-X: Enable+ Count=16 Masked-
Vector table: BAR=0 offset=00002000
PBA: BAR=0 offset=00002100
Capabilities: [100 v2] Advanced Error Reporting
UESta: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UEMsk: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
CESta: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
CEMsk: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
AERCap: First Error Pointer: 00, GenCap+ CGenEn- ChkCap+ ChkEn-
Capabilities: [158 v1] #19
Capabilities: [178 v1] Latency Tolerance Reporting
Max snoop latency: 71680ns
Max no snoop latency: 71680ns
Capabilities: [180 v1] L1 PM Substates
L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
PortCommonModeRestoreTime=10us PortTPowerOnTime=10us
L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
T_CommonMode=0us LTR1.2_Threshold=0ns
L1SubCtl2: T_PwrOn=10us
Kernel driver in use: nvme
Kernel modules: nvme

3-2) iozone
Iozone: Performance Test of File I/O
Version $Revision: 3.429 $
Compiled for 64 bit mode.
Build: linux-AMD64

Contributors:William Norcott, Don Capps, Isom Crawford, Kirby Collins
Al Slater, Scott Rhine, Mike Wisner, Ken Goss
Steve Landherr, Brad Smith, Mark Kelly, Dr. Alain CYR,
Randy Dunlap, Mark Montague, Dan Million, Gavin Brebner,
Jean-Marc Zucconi, Jeff Blomberg, Benny Halevy, Dave Boone,
Erik Habbinga, Kris Strecker, Walter Wong, Joshua Root,
Fabrice Bacchella, Zhenghua Xue, Qin Li, Darren Sawyer,
Vangel Bojaxhi, Ben England, Vikentsi Lapa.

Run began: Mon Jan 16 13:17:46 2023

Record Size 4 kB
Record Size 8 kB
Record Size 64 kB
Record Size 256 kB
Record Size 512 kB
Record Size 1024 kB
Record Size 2048 kB
Record Size 4096 kB
SYNC Mode.
O_DIRECT feature enabled
File size set to 10240 kB
Command line used: iozone -r 4k -r 8k -r 64k -r 256k -r 512k -r 1024k -r 2048k -r 4096k -o -i 0 -i 1 -i 2 -I -s 10m -f /mnt/nvme/iozone
Output is in kBytes/sec
Time Resolution = 0.000001 seconds.
Processor cache size set to 1024 kBytes.
Processor cache line size set to 32 bytes.
File stride size set to 17 * record size.
random random bkwd record stride
kB reclen write rewrite read reread read write read rewrite read fwrite frewrite fread freread
10240 4 1075 1157 150030 150180 54507 5202
10240 8 3469 2303 262496 285069 96336 15991
10240 64 16714 19461 1093428 1095436 323948 80137
10240 256 67094 64389 1126731 1171478 663174 64499
10240 512 129927 130592 1210675 1218610 968407 124367
10240 1024 251244 271328 1340844 1351434 1213960 448945
10240 2048 432778 615714 1439582 1440017 1044272 533802
10240 4096 829488 520990 1483529 1466496 1007504 567312

iozone test complete.

3-3) hdparm
/dev/nvme0n1:
Timing buffered disk reads: 4464 MB in 3.00 seconds = 1487.96 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4456 MB in 3.00 seconds = 1484.83 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4626 MB in 3.00 seconds = 1541.65 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4328 MB in 3.00 seconds = 1442.18 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 3538 MB in 3.00 seconds = 1179.32 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4280 MB in 3.00 seconds = 1426.45 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4646 MB in 3.00 seconds = 1548.14 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4442 MB in 3.00 seconds = 1480.39 MB/sec

/dev/nvme0n1:
Timing buffered disk reads: 4644 MB in 3.00 seconds = 1547.91 MB/sec

4. retimer EEROM and Register dump
1) EEPROM
:20000000220000041D030000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFB2
:20002000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFE0
:20004000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFC0
:20006000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFA0
:20008000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF80
:2000A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF60
:2000C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF40
:2000E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF20
:20010000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF
:20012000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDF
:20014000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBF
:20016000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9F
:20018000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7F
:2001A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5F
:2001C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3F
:2001E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1F
:20020000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFE
:20022000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDE
:20024000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBE
:20026000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9E
:20028000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7E
:2002A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5E
:2002C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3E
:2002E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1E
:20030000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFD
:20032000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDD
:20034000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBD
:20036000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9D
:20038000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7D
:2003A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5D
:2003C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3D
:2003E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1D
:20040000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFC
:20042000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDC
:20044000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBC
:20046000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9C
:20048000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7C
:2004A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5C
:2004C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3C
:2004E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1C
:20050000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFB
:20052000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDB
:20054000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBB
:20056000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9B
:20058000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7B
:2005A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5B
:2005C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3B
:2005E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1B
:20060000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFA
:20062000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDA
:20064000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBA
:20066000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9A
:20068000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7A
:2006A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5A
:2006C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3A
:2006E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1A
:20070000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9
:20072000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFD9
:20074000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFB9
:20076000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF99
:20078000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF79
:2007A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF59
:2007C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF39
:2007E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF000017
:00000001FF

2) Register
0xF0 Global Registers_reg_F0 01 01
0xF1 Global Registers_reg_F1 24 24
0xF2 Global Registers_reg_F2 01 01
0xF3 Global Registers_reg_F3 80 A0
0xF4 Global Registers_reg_F4 00 00
0xF5 Global Registers_reg_F5 00 00
0xF6 Global Registers_reg_F6 72 72
0xF7 Global Registers_reg_F7 41 41
0xF8 Global Registers_reg_F8 01 01
0xF9 Global Registers_reg_F9 00 00
0xFA Global Registers_reg_FA 00 00
0xFB Global Registers_reg_FB 01 01
0xFC Global Registers_reg_FC 00 00
0xFD Global Registers_reg_FD 00 00
0xFE Global Registers_reg_FE 24 24
0xFF Global Registers_reg_FF 90 90
0x0 Die0 Shared Registers_reg_00 00 00
0x1 Die0 Shared Registers_reg_01 00 00
0x2 Die0 Shared Registers_reg_02 00 00
0x3 Die0 Shared Registers_reg_03 01 01
0x4 Die0 Shared Registers_reg_04 00 00
0x5 Die0 Shared Registers_reg_05 00 00
0x6 Die0 Shared Registers_reg_06 04 04
0x7 Die0 Shared Registers_reg_07 12 12
0x8 Die0 Shared Registers_reg_08 00 00
0x9 Die0 Shared Registers_reg_09 00 00
0xA Die0 Shared Registers_reg_0A FF FF
0xB Die0 Shared Registers_reg_0B FF FF
0xC Die0 Shared Registers_reg_0C FF FF
0xD Die0 Shared Registers_reg_0D D0 D0
0xE Die0 Shared Registers_reg_0E 11 00
0xF Die0 Shared Registers_reg_0F 00 00
0x10 Die0 Shared Registers_reg_10 00 00
0x11 Die0 Shared Registers_reg_11 00 00
0x12 Die0 Shared Registers_reg_12 22 26
0x13 Die0 Shared Registers_reg_13 00 00
0x14 Die0 Shared Registers_reg_14 00 00
0x15 Die0 Shared Registers_reg_15 00 00
0x16 Die0 Shared Registers_reg_16 00 00
0x17 Die0 Shared Registers_reg_17 00 00
0x18 Die0 Shared Registers_reg_18 D0 D0
0x19 Die0 Shared Registers_reg_19 A0 A0
0x1A Die0 Shared Registers_reg_1A 00 00
0x1B Die0 Shared Registers_reg_1B 00 00
0x1C Die0 Shared Registers_reg_1C 40 40
0x1D Die0 Shared Registers_reg_1D 28 28
0x1E Die0 Shared Registers_reg_1E A0 A0
0x1F Die0 Shared Registers_reg_1F 00 20
0x20 Die0 Shared Registers_reg_20 00 00
0x21 Die0 Shared Registers_reg_21 00 00
0x22 Die0 Shared Registers_reg_22 33 33
0x23 Die0 Shared Registers_reg_23 00 00
0x24 Die0 Shared Registers_reg_24 02 02
0x25 Die0 Shared Registers_reg_25 00 00
0x26 Die0 Shared Registers_reg_26 3E 3D
0x27 Die0 Shared Registers_reg_27 00 00
0x28 Die0 Shared Registers_reg_28 00 00
0x29 Die0 Shared Registers_reg_29 00 00
0x2A Die0 Shared Registers_reg_2A 00 00
0x2B Die0 Shared Registers_reg_2B 00 00
0x2C Die0 Shared Registers_reg_2C 00 00
0x2D Die0 Shared Registers_reg_2D 00 00
0x2E Die0 Shared Registers_reg_2E 00 00
0x2F Die0 Shared Registers_reg_2F 00 00
0x30 Die0 Shared Registers_reg_30 00 00
0x31 Die0 Shared Registers_reg_31 04 04
0x32 Die0 Shared Registers_reg_32 6B 6B
0x33 Die0 Shared Registers_reg_33 25 25
0x34 Die0 Shared Registers_reg_34 02 02
0x35 Die0 Shared Registers_reg_35 7B 7B
0x36 Die0 Shared Registers_reg_36 23 23
0x37 Die0 Shared Registers_reg_37 01 01
0x38 Die0 Shared Registers_reg_38 6B 6B
0x39 Die0 Shared Registers_reg_39 25 25
0x3A Die0 Shared Registers_reg_3A 02 02
0x3B Die0 Shared Registers_reg_3B 7B 7B
0x3C Die0 Shared Registers_reg_3C 23 23
0x3D Die0 Shared Registers_reg_3D 01 01
0x3E Die0 Shared Registers_reg_3E 14 14
0x3F Die0 Shared Registers_reg_3F 00 00
0x40 Die0 Shared Registers_reg_40 00 00
0x41 Die0 Shared Registers_reg_41 00 00
0x42 Die0 Shared Registers_reg_42 E4 E4
0x43 Die0 Shared Registers_reg_43 51 51
0x44 Die0 Shared Registers_reg_44 51 51
0x45 Die0 Shared Registers_reg_45 51 51
0x46 Die0 Shared Registers_reg_46 53 53
0x47 Die0 Shared Registers_reg_47 00 00
0x48 Die0 Shared Registers_reg_48 00 00
0x49 Die0 Shared Registers_reg_49 00 00
0x4A Die0 Shared Registers_reg_4A 00 00
0x4B Die0 Shared Registers_reg_4B 00 00
0x4C Die0 Shared Registers_reg_4C 00 00
0x4D Die0 Shared Registers_reg_4D 00 00
0x4E Die0 Shared Registers_reg_4E 00 00
0x4F Die0 Shared Registers_reg_4F 2D 2D
0x50 Die0 Shared Registers_reg_50 00 00
0x51 Die0 Shared Registers_reg_51 20 20
0x52 Die0 Shared Registers_reg_52 80 80
0x53 Die0 Shared Registers_reg_53 01 01
0x54 Die0 Shared Registers_reg_54 7E 7E
0x55 Die0 Shared Registers_reg_55 64 64
0x56 Die0 Shared Registers_reg_56 80 80
0x57 Die0 Shared Registers_reg_57 1C 1C
0x58 Die0 Shared Registers_reg_58 80 80
0x59 Die0 Shared Registers_reg_59 16 16
0x5A Die0 Shared Registers_reg_5A 00 00
0x5B Die0 Shared Registers_reg_5B 04 04
0x5C Die0 Shared Registers_reg_5C 00 00
0x5D Die0 Shared Registers_reg_5D 05 05
0x5E Die0 Shared Registers_reg_5E 00 00
0x5F Die0 Shared Registers_reg_5F 00 00
0x60 Die0 Shared Registers_reg_60 80 80
0x61 Die0 Shared Registers_reg_61 00 00
0x62 Die0 Shared Registers_reg_62 00 00
0x63 Die0 Shared Registers_reg_63 00 00
0x64 Die0 Shared Registers_reg_64 00 00
0x65 Die0 Shared Registers_reg_65 58 58
0x66 Die0 Shared Registers_reg_66 77 77
0x67 Die0 Shared Registers_reg_67 10 10
0x68 Die0 Shared Registers_reg_68 00 00
0x69 Die0 Shared Registers_reg_69 2C 2C
0x6A Die0 Shared Registers_reg_6A 00 00
0x6B Die0 Shared Registers_reg_6B 00 00
0x6C Die0 Shared Registers_reg_6C 00 00
0x6D Die0 Shared Registers_reg_6D 00 00
0x6E Die0 Shared Registers_reg_6E 00 00
0x6F Die0 Shared Registers_reg_6F 00 00
0x70 Die0 Shared Registers_reg_70 00 00
0x71 Die0 Shared Registers_reg_71 00 00
0x72 Die0 Shared Registers_reg_72 00 00
0x73 Die0 Shared Registers_reg_73 20 20
0x74 Die0 Shared Registers_reg_74 FF FF
0x75 Die0 Shared Registers_reg_75 FF FF
0x76 Die0 Shared Registers_reg_76 0C 0C
0x77 Die0 Shared Registers_reg_77 00 00
0x78 Die0 Shared Registers_reg_78 00 00
0x79 Die0 Shared Registers_reg_79 00 01
0x7A Die0 Shared Registers_reg_7A 00 00
0x7B Die0 Shared Registers_reg_7B 00 00
0x7C Die0 Shared Registers_reg_7C 00 DF
0x7D Die0 Shared Registers_reg_7D 10 47
0x7E Die0 Shared Registers_reg_7E 00 CA
0x7F Die0 Shared Registers_reg_7F 10 43
0x80 Die0 Shared Registers_reg_80 00 BB
0x81 Die0 Shared Registers_reg_81 8D 71
0x82 Die0 Shared Registers_reg_82 66 66
0x83 Die0 Shared Registers_reg_83 07 01
0x84 Die0 Shared Registers_reg_84 38 00
0x85 Die0 Shared Registers_reg_85 8D 7C
0x86 Die0 Shared Registers_reg_86 66 66
0x87 Die0 Shared Registers_reg_87 00 00
0x88 Die0 Shared Registers_reg_88 00 00
0x89 Die0 Shared Registers_reg_89 00 00
0x8A Die0 Shared Registers_reg_8A 00 00
0x8B Die0 Shared Registers_reg_8B 00 00
0x8C Die0 Shared Registers_reg_8C 00 00
0x8D Die0 Shared Registers_reg_8D 00 00
0x8E Die0 Shared Registers_reg_8E 00 00
0x8F Die0 Shared Registers_reg_8F 00 00
0x90 Die0 Shared Registers_reg_90 03 0C
0x91 Die0 Shared Registers_reg_91 27 27
0x92 Die0 Shared Registers_reg_92 11 11
0x93 Die0 Shared Registers_reg_93 03 03
0x94 Die0 Shared Registers_reg_94 00 00
0x95 Die0 Shared Registers_reg_95 1A 1A
0x96 Die0 Shared Registers_reg_96 08 08
0x97 Die0 Shared Registers_reg_97 1A 1A
0x98 Die0 Shared Registers_reg_98 08 08
0x99 Die0 Shared Registers_reg_99 00 00
0x9A Die0 Shared Registers_reg_9A 00 00
0x9B Die0 Shared Registers_reg_9B 00 00
0x9C Die0 Shared Registers_reg_9C FA FA
0x9D Die0 Shared Registers_reg_9D 03 03
0x9E Die0 Shared Registers_reg_9E D8 D8
0x9F Die0 Shared Registers_reg_9F 00 00
0xA0 Die0 Shared Registers_reg_A0 10 10
0xA1 Die0 Shared Registers_reg_A1 21 21
0xA2 Die0 Shared Registers_reg_A2 22 22
0xA3 Die0 Shared Registers_reg_A3 33 33
0xA4 Die0 Shared Registers_reg_A4 33 33
0xA5 Die0 Shared Registers_reg_A5 64 64
0xA6 Die0 Shared Registers_reg_A6 00 00
0xA7 Die0 Shared Registers_reg_A7 11 11
0xA8 Die0 Shared Registers_reg_A8 21 21
0xA9 Die0 Shared Registers_reg_A9 22 22
0xAA Die0 Shared Registers_reg_AA 43 43
0xAB Die0 Shared Registers_reg_AB 65 65
0xAC Die0 Shared Registers_reg_AC 00 00
0xAD Die0 Shared Registers_reg_AD 00 00
0xAE Die0 Shared Registers_reg_AE 20 E0
0xAF Die0 Shared Registers_reg_AF D1 D4
0xB0 Die0 Shared Registers_reg_B0 10 10
0xB1 Die0 Shared Registers_reg_B1 21 21
0xB2 Die0 Shared Registers_reg_B2 33 33
0xB3 Die0 Shared Registers_reg_B3 85 85
0xB4 Die0 Shared Registers_reg_B4 B9 B9
0xB5 Die0 Shared Registers_reg_B5 FD FD
0xB6 Die0 Shared Registers_reg_B6 46 46
0xB7 Die0 Shared Registers_reg_B7 69 00
0xB8 Die0 Shared Registers_reg_B8 02 02
0xB9 Die0 Shared Registers_reg_B9 00 00
0xBA Die0 Shared Registers_reg_BA 00 00
0xBB Die0 Shared Registers_reg_BB 00 00
0xBC Die0 Shared Registers_reg_BC 00 00
0xBD Die0 Shared Registers_reg_BD 00 00
0xBE Die0 Shared Registers_reg_BE 00 00
0xBF Die0 Shared Registers_reg_BF 06 02
0xC0 Die0 Shared Registers_reg_C0 82 00
0xC1 Die0 Shared Registers_reg_C1 02 48
0xC2 Die0 Shared Registers_reg_C2 BE BE
0xC3 Die0 Shared Registers_reg_C3 00 00
0xC4 Die0 Shared Registers_reg_C4 98 98
0xC5 Die0 Shared Registers_reg_C5 02 02
0xC6 Die0 Shared Registers_reg_C6 10 10
0xC7 Die0 Shared Registers_reg_C7 13 13
0xC8 Die0 Shared Registers_reg_C8 8A 8A
0xC9 Die0 Shared Registers_reg_C9 7F 7F
0xCA Die0 Shared Registers_reg_CA 1F 1F
0xCB Die0 Shared Registers_reg_CB 80 80
0xCC Die0 Shared Registers_reg_CC 80 80
0xCD Die0 Shared Registers_reg_CD 80 80
0xCE Die0 Shared Registers_reg_CE 02 02
0xCF Die0 Shared Registers_reg_CF 7F 7F
0xD0 Die0 Shared Registers_reg_D0 1F 1F
0xD1 Die0 Shared Registers_reg_D1 80 80
0xD2 Die0 Shared Registers_reg_D2 80 80
0xD3 Die0 Shared Registers_reg_D3 80 80
0xD4 Die0 Shared Registers_reg_D4 02 02
0xD5 Die0 Shared Registers_reg_D5 00 00
0xD6 Die0 Shared Registers_reg_D6 04 07
0xD7 Die0 Shared Registers_reg_D7 1A 1A
0xD8 Die0 Shared Registers_reg_D8 1A 1A
0xD9 Die0 Shared Registers_reg_D9 06 06
0xDA Die0 Shared Registers_reg_DA 00 02
0xDB Die0 Shared Registers_reg_DB 09 09
0xDC Die0 Shared Registers_reg_DC 04 04
0xDD Die0 Shared Registers_reg_DD 35 35
0xDE Die0 Shared Registers_reg_DE 08 18
0xDF Die0 Shared Registers_reg_DF 08 18
0xE0 Die0 Shared Registers_reg_E0 01 02
0xE1 Die0 Shared Registers_reg_E1 03 00
0xE2 Die0 Shared Registers_reg_E2 03 03
0xE3 Die0 Shared Registers_reg_E3 00 00
0xE4 Die0 Shared Registers_reg_E4 00 00
0xE5 Die0 Shared Registers_reg_E5 00 00
0xE6 Die0 Shared Registers_reg_E6 00 00
0xE7 Die0 Shared Registers_reg_E7 00 00
0xE8 Die0 Shared Registers_reg_E8 20 20
0xE9 Die0 Shared Registers_reg_E9 00 00
0xEA Die0 Shared Registers_reg_EA 00 00
0xEB Die0 Shared Registers_reg_EB 00 00
0xEC Die0 Shared Registers_reg_EC 00 00
0xED Die0 Shared Registers_reg_ED 00 00
0xEE Die0 Shared Registers_reg_EE 00 00
0xEF Die0 Shared Registers_reg_EF 0C 0C
0x0 Die1 Shared Registers_reg_00 00 00
0x1 Die1 Shared Registers_reg_01 00 00
0x2 Die1 Shared Registers_reg_02 00 00
0x3 Die1 Shared Registers_reg_03 01 01
0x4 Die1 Shared Registers_reg_04 00 00
0x5 Die1 Shared Registers_reg_05 00 00
0x6 Die1 Shared Registers_reg_06 04 04
0x7 Die1 Shared Registers_reg_07 12 12
0x8 Die1 Shared Registers_reg_08 00 00
0x9 Die1 Shared Registers_reg_09 00 00
0xA Die1 Shared Registers_reg_0A FF FF
0xB Die1 Shared Registers_reg_0B FF FF
0xC Die1 Shared Registers_reg_0C FF FF
0xD Die1 Shared Registers_reg_0D D0 D0
0xE Die1 Shared Registers_reg_0E 00 00
0xF Die1 Shared Registers_reg_0F 00 00
0x10 Die1 Shared Registers_reg_10 00 00
0x11 Die1 Shared Registers_reg_11 00 00
0x12 Die1 Shared Registers_reg_12 28 28
0x13 Die1 Shared Registers_reg_13 00 00
0x14 Die1 Shared Registers_reg_14 00 00
0x15 Die1 Shared Registers_reg_15 00 00
0x16 Die1 Shared Registers_reg_16 00 00
0x17 Die1 Shared Registers_reg_17 00 00
0x18 Die1 Shared Registers_reg_18 D0 D0
0x19 Die1 Shared Registers_reg_19 A0 A0
0x1A Die1 Shared Registers_reg_1A 00 00
0x1B Die1 Shared Registers_reg_1B 00 00
0x1C Die1 Shared Registers_reg_1C 80 80
0x1D Die1 Shared Registers_reg_1D 28 28
0x1E Die1 Shared Registers_reg_1E A0 A0
0x1F Die1 Shared Registers_reg_1F 00 20
0x20 Die1 Shared Registers_reg_20 00 00
0x21 Die1 Shared Registers_reg_21 00 00
0x22 Die1 Shared Registers_reg_22 33 33
0x23 Die1 Shared Registers_reg_23 00 00
0x24 Die1 Shared Registers_reg_24 02 02
0x25 Die1 Shared Registers_reg_25 00 00
0x26 Die1 Shared Registers_reg_26 3E 3E
0x27 Die1 Shared Registers_reg_27 00 00
0x28 Die1 Shared Registers_reg_28 00 00
0x29 Die1 Shared Registers_reg_29 00 00
0x2A Die1 Shared Registers_reg_2A 00 00
0x2B Die1 Shared Registers_reg_2B 00 00
0x2C Die1 Shared Registers_reg_2C 00 00
0x2D Die1 Shared Registers_reg_2D 00 00
0x2E Die1 Shared Registers_reg_2E 00 00
0x2F Die1 Shared Registers_reg_2F 00 00
0x30 Die1 Shared Registers_reg_30 00 00
0x31 Die1 Shared Registers_reg_31 04 04
0x32 Die1 Shared Registers_reg_32 6B 6B
0x33 Die1 Shared Registers_reg_33 25 25
0x34 Die1 Shared Registers_reg_34 02 02
0x35 Die1 Shared Registers_reg_35 7B 7B
0x36 Die1 Shared Registers_reg_36 23 23
0x37 Die1 Shared Registers_reg_37 01 01
0x38 Die1 Shared Registers_reg_38 6B 6B
0x39 Die1 Shared Registers_reg_39 25 25
0x3A Die1 Shared Registers_reg_3A 02 02
0x3B Die1 Shared Registers_reg_3B 7B 7B
0x3C Die1 Shared Registers_reg_3C 23 23
0x3D Die1 Shared Registers_reg_3D 01 01
0x3E Die1 Shared Registers_reg_3E 14 14
0x3F Die1 Shared Registers_reg_3F 00 00
0x40 Die1 Shared Registers_reg_40 00 00
0x41 Die1 Shared Registers_reg_41 00 00
0x42 Die1 Shared Registers_reg_42 E4 E4
0x43 Die1 Shared Registers_reg_43 51 51
0x44 Die1 Shared Registers_reg_44 51 51
0x45 Die1 Shared Registers_reg_45 51 51
0x46 Die1 Shared Registers_reg_46 53 53
0x47 Die1 Shared Registers_reg_47 00 00
0x48 Die1 Shared Registers_reg_48 00 00
0x49 Die1 Shared Registers_reg_49 00 00
0x4A Die1 Shared Registers_reg_4A 00 00
0x4B Die1 Shared Registers_reg_4B 00 00
0x4C Die1 Shared Registers_reg_4C 00 00
0x4D Die1 Shared Registers_reg_4D 00 00
0x4E Die1 Shared Registers_reg_4E 00 00
0x4F Die1 Shared Registers_reg_4F 2D 2D
0x50 Die1 Shared Registers_reg_50 00 00
0x51 Die1 Shared Registers_reg_51 20 20
0x52 Die1 Shared Registers_reg_52 80 80
0x53 Die1 Shared Registers_reg_53 01 01
0x54 Die1 Shared Registers_reg_54 7E 7E
0x55 Die1 Shared Registers_reg_55 64 64
0x56 Die1 Shared Registers_reg_56 80 80
0x57 Die1 Shared Registers_reg_57 1C 1C
0x58 Die1 Shared Registers_reg_58 80 80
0x59 Die1 Shared Registers_reg_59 16 16
0x5A Die1 Shared Registers_reg_5A 00 00
0x5B Die1 Shared Registers_reg_5B 04 04
0x5C Die1 Shared Registers_reg_5C 00 00
0x5D Die1 Shared Registers_reg_5D 05 05
0x5E Die1 Shared Registers_reg_5E 00 00
0x5F Die1 Shared Registers_reg_5F 00 00
0x60 Die1 Shared Registers_reg_60 80 80
0x61 Die1 Shared Registers_reg_61 00 00
0x62 Die1 Shared Registers_reg_62 00 00
0x63 Die1 Shared Registers_reg_63 00 00
0x64 Die1 Shared Registers_reg_64 00 00
0x65 Die1 Shared Registers_reg_65 58 58
0x66 Die1 Shared Registers_reg_66 77 77
0x67 Die1 Shared Registers_reg_67 10 10
0x68 Die1 Shared Registers_reg_68 00 00
0x69 Die1 Shared Registers_reg_69 2C 2C
0x6A Die1 Shared Registers_reg_6A 00 00
0x6B Die1 Shared Registers_reg_6B 00 00
0x6C Die1 Shared Registers_reg_6C 00 00
0x6D Die1 Shared Registers_reg_6D 00 00
0x6E Die1 Shared Registers_reg_6E 00 00
0x6F Die1 Shared Registers_reg_6F 00 00
0x70 Die1 Shared Registers_reg_70 00 00
0x71 Die1 Shared Registers_reg_71 00 00
0x72 Die1 Shared Registers_reg_72 00 00
0x73 Die1 Shared Registers_reg_73 20 20
0x74 Die1 Shared Registers_reg_74 FF FF
0x75 Die1 Shared Registers_reg_75 FF FF
0x76 Die1 Shared Registers_reg_76 0C 0C
0x77 Die1 Shared Registers_reg_77 00 00
0x78 Die1 Shared Registers_reg_78 00 00
0x79 Die1 Shared Registers_reg_79 00 00
0x7A Die1 Shared Registers_reg_7A 00 00
0x7B Die1 Shared Registers_reg_7B 00 00
0x7C Die1 Shared Registers_reg_7C 08 44
0x7D Die1 Shared Registers_reg_7D 10 3B
0x7E Die1 Shared Registers_reg_7E 00 CE
0x7F Die1 Shared Registers_reg_7F 10 3D
0x80 Die1 Shared Registers_reg_80 00 B5
0x81 Die1 Shared Registers_reg_81 8D 77
0x82 Die1 Shared Registers_reg_82 66 66
0x83 Die1 Shared Registers_reg_83 07 01
0x84 Die1 Shared Registers_reg_84 38 00
0x85 Die1 Shared Registers_reg_85 8D 7C
0x86 Die1 Shared Registers_reg_86 66 66
0x87 Die1 Shared Registers_reg_87 00 00
0x88 Die1 Shared Registers_reg_88 00 00
0x89 Die1 Shared Registers_reg_89 00 00
0x8A Die1 Shared Registers_reg_8A 00 00
0x8B Die1 Shared Registers_reg_8B 00 00
0x8C Die1 Shared Registers_reg_8C 00 00
0x8D Die1 Shared Registers_reg_8D 00 00
0x8E Die1 Shared Registers_reg_8E 00 00
0x8F Die1 Shared Registers_reg_8F 00 00
0x90 Die1 Shared Registers_reg_90 0C 0C
0x91 Die1 Shared Registers_reg_91 27 27
0x92 Die1 Shared Registers_reg_92 11 11
0x93 Die1 Shared Registers_reg_93 03 03
0x94 Die1 Shared Registers_reg_94 00 00
0x95 Die1 Shared Registers_reg_95 1A 1A
0x96 Die1 Shared Registers_reg_96 08 08
0x97 Die1 Shared Registers_reg_97 1A 1A
0x98 Die1 Shared Registers_reg_98 08 08
0x99 Die1 Shared Registers_reg_99 00 00
0x9A Die1 Shared Registers_reg_9A 00 00
0x9B Die1 Shared Registers_reg_9B 00 00
0x9C Die1 Shared Registers_reg_9C FA FA
0x9D Die1 Shared Registers_reg_9D 03 03
0x9E Die1 Shared Registers_reg_9E D8 D8
0x9F Die1 Shared Registers_reg_9F 00 00
0xA0 Die1 Shared Registers_reg_A0 10 10
0xA1 Die1 Shared Registers_reg_A1 21 21
0xA2 Die1 Shared Registers_reg_A2 22 22
0xA3 Die1 Shared Registers_reg_A3 33 33
0xA4 Die1 Shared Registers_reg_A4 33 33
0xA5 Die1 Shared Registers_reg_A5 64 64
0xA6 Die1 Shared Registers_reg_A6 00 00
0xA7 Die1 Shared Registers_reg_A7 11 11
0xA8 Die1 Shared Registers_reg_A8 21 21
0xA9 Die1 Shared Registers_reg_A9 22 22
0xAA Die1 Shared Registers_reg_AA 43 43
0xAB Die1 Shared Registers_reg_AB 65 65
0xAC Die1 Shared Registers_reg_AC 00 00
0xAD Die1 Shared Registers_reg_AD 00 00
0xAE Die1 Shared Registers_reg_AE 20 E0
0xAF Die1 Shared Registers_reg_AF D1 D4
0xB0 Die1 Shared Registers_reg_B0 10 10
0xB1 Die1 Shared Registers_reg_B1 21 21
0xB2 Die1 Shared Registers_reg_B2 33 33
0xB3 Die1 Shared Registers_reg_B3 85 85
0xB4 Die1 Shared Registers_reg_B4 B9 B9
0xB5 Die1 Shared Registers_reg_B5 FD FD
0xB6 Die1 Shared Registers_reg_B6 46 46
0xB7 Die1 Shared Registers_reg_B7 69 00
0xB8 Die1 Shared Registers_reg_B8 02 02
0xB9 Die1 Shared Registers_reg_B9 00 00
0xBA Die1 Shared Registers_reg_BA 00 00
0xBB Die1 Shared Registers_reg_BB 00 00
0xBC Die1 Shared Registers_reg_BC 00 00
0xBD Die1 Shared Registers_reg_BD 00 00
0xBE Die1 Shared Registers_reg_BE 00 00
0xBF Die1 Shared Registers_reg_BF 06 02
0xC0 Die1 Shared Registers_reg_C0 00 00
0xC1 Die1 Shared Registers_reg_C1 48 48
0xC2 Die1 Shared Registers_reg_C2 BE BE
0xC3 Die1 Shared Registers_reg_C3 00 00
0xC4 Die1 Shared Registers_reg_C4 98 98
0xC5 Die1 Shared Registers_reg_C5 02 02
0xC6 Die1 Shared Registers_reg_C6 10 10
0xC7 Die1 Shared Registers_reg_C7 13 13
0xC8 Die1 Shared Registers_reg_C8 8A 8A
0xC9 Die1 Shared Registers_reg_C9 7F 7F
0xCA Die1 Shared Registers_reg_CA 1F 1F
0xCB Die1 Shared Registers_reg_CB 80 80
0xCC Die1 Shared Registers_reg_CC 80 80
0xCD Die1 Shared Registers_reg_CD 80 80
0xCE Die1 Shared Registers_reg_CE 02 02
0xCF Die1 Shared Registers_reg_CF 7F 7F
0xD0 Die1 Shared Registers_reg_D0 1F 1F
0xD1 Die1 Shared Registers_reg_D1 80 80
0xD2 Die1 Shared Registers_reg_D2 80 80
0xD3 Die1 Shared Registers_reg_D3 80 80
0xD4 Die1 Shared Registers_reg_D4 02 02
0xD5 Die1 Shared Registers_reg_D5 00 00
0xD6 Die1 Shared Registers_reg_D6 04 07
0xD7 Die1 Shared Registers_reg_D7 1A 1A
0xD8 Die1 Shared Registers_reg_D8 1A 1A
0xD9 Die1 Shared Registers_reg_D9 06 06
0xDA Die1 Shared Registers_reg_DA 00 02
0xDB Die1 Shared Registers_reg_DB 09 09
0xDC Die1 Shared Registers_reg_DC 04 04
0xDD Die1 Shared Registers_reg_DD 35 35
0xDE Die1 Shared Registers_reg_DE 08 18
0xDF Die1 Shared Registers_reg_DF 08 18
0xE0 Die1 Shared Registers_reg_E0 01 02
0xE1 Die1 Shared Registers_reg_E1 03 00
0xE2 Die1 Shared Registers_reg_E2 03 03
0xE3 Die1 Shared Registers_reg_E3 00 00
0xE4 Die1 Shared Registers_reg_E4 00 00
0xE5 Die1 Shared Registers_reg_E5 00 00
0xE6 Die1 Shared Registers_reg_E6 00 00
0xE7 Die1 Shared Registers_reg_E7 00 00
0xE8 Die1 Shared Registers_reg_E8 20 20
0xE9 Die1 Shared Registers_reg_E9 00 00
0xEA Die1 Shared Registers_reg_EA 00 00
0xEB Die1 Shared Registers_reg_EB 00 00
0xEC Die1 Shared Registers_reg_EC 00 00
0xED Die1 Shared Registers_reg_ED 00 00
0xEE Die1 Shared Registers_reg_EE 00 00
0xEF Die1 Shared Registers_reg_EF 0C 0C
0x0 Rx/Tx A0_reg_00 00 00
0x1 Rx/Tx A0_reg_01 00 00
0x2 Rx/Tx A0_reg_02 00 00
0x3 Rx/Tx A0_reg_03 00 00
0x4 Rx/Tx A0_reg_04 BE BE
0x5 Rx/Tx A0_reg_05 00 00
0x6 Rx/Tx A0_reg_06 00 00
0x7 Rx/Tx A0_reg_07 03 03
0x8 Rx/Tx A0_reg_08 00 00
0x9 Rx/Tx A0_reg_09 00 00
0xA Rx/Tx A0_reg_0A 00 00
0xB Rx/Tx A0_reg_0B 00 00
0xC Rx/Tx A0_reg_0C 00 00
0xD Rx/Tx A0_reg_0D 00 00
0xE Rx/Tx A0_reg_0E 07 07
0xF Rx/Tx A0_reg_0F 81 C4
0x10 Rx/Tx A0_reg_10 81 81
0x11 Rx/Tx A0_reg_11 C2 81
0x12 Rx/Tx A0_reg_12 C2 C1
0x13 Rx/Tx A0_reg_13 82 82
0x14 Rx/Tx A0_reg_14 C0 82
0x15 Rx/Tx A0_reg_15 86 C0
0x16 Rx/Tx A0_reg_16 83 84
0x17 Rx/Tx A0_reg_17 C2 C2
0x18 Rx/Tx A0_reg_18 C3 C0
0x19 Rx/Tx A0_reg_19 83 81
0x1A Rx/Tx A0_reg_1A 86 81
0x1B Rx/Tx A0_reg_1B 7A 99
0x1C Rx/Tx A0_reg_1C 08 0B
0x1D Rx/Tx A0_reg_1D 00 00
0x1E Rx/Tx A0_reg_1E 00 00
0x1F Rx/Tx A0_reg_1F 00 00
0x20 Rx/Tx A0_reg_20 00 00
0x21 Rx/Tx A0_reg_21 00 00
0x22 Rx/Tx A0