In DS90UB953A-Q1 data sheet, it mention that
1. FPD-Link III 4.16-Gbps Serializer with CSI-2 Interface for 2.3MP/60fps Cameras
2. D-PHY v1.2 and CSI-2 v1.3 compliant system interface Up to 4 data lanes at 832 Mbps per each lane.
If a camera with resolution 1900x1600 RAW10 60fps and MIPI data rate is 800Mbps @ 4 lanes,
this is 3MP/60 fps camera > 2.3MP/60fps but its MIPI output data rate is under 832Mbps (max bandwidth DS90UB953A-Q1 can support),
can I say this camera can be supported by the DS90UB953 ?
I mean that if a CSI-Camera with mipi output data stream < 832 Mbps , then I can say the camera can be compatiable with UB953 regardless of its resolution ?
thanks