This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042G-Q1:About the applied voltage of the power supply.

Part Number: TCAN1042G-Q1

Is there any rating problem with the operation of applying 5V to VIO and 3.3V to VCC?

  • Hi User,

    The TCAN1042 requires that Vcc be above 4.5V in order to operate as specified. If the Vcc voltage is below this level, the datasheet specified operation is not guaranteed. 

    The Vcc and Vio supplies have independant references to ground, so there is no issue electrically if the voltages are connected in this way from a device damage standpoint. 

    Let me know if you have any more questions.

    Regards,
    Eric Schott