Hello,
I am using this obsolete IC to scan a keypad. IC - MM74C922WM.
Do you carry an IC where I can read a 4 x 4 keypad?
I need the response as bits and not I2C as there is no I2C/SPI bus in this design.
Regards,
Divakar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is no similar device. Nowadays, this is done with I²C or more often with the microcontroller.
Hello,
To add to this, we have some reference designs for keypads using our inductive sensing devices. Devices like the LDC3114 still use I2C but only need to be configured at startup and then can provide digital outputs for the button presses.
Best Regards,
Justin Beigel