This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD73: supply voltage

Part Number: SN65HVD73
Other Parts Discussed in Thread: THVD1424

SN65HVD7x supply voltage use 2.5V.

WE use vcc2.5v can work normally. I want to know the risk of using it on 2.5v

  • The minimum recommended supply voltage is 3 V. At lower voltages, correct operation is not guaranteed.

    There are RS-485 transceivers with integrated level shifters for the logic signals like the THVD1424, but they still need a 3.3 V supply to generate the bus voltages.

  • Hi Daniel,

    Unfortunately, this part is rated to function at a minimum of 3 V. There is a chance that it won't read logic levels or function properly with a VCC of only 2.5 V.

    Please reach out with anything else.

    Zach