Part Number: TUSB8041A
Other Parts Discussed in Thread: TUSB8041, TUSB8041EVM
Hi everyone, sorry for my poor english.
I use TUSB8041 for a TYPE-C dock design , type-c port convert to HDMI+USB 3.0( x4-port)+RJ45 100M network port.
4 USB 3.0 port+1 RJ45 100 M network ports i use 2 TUSB8041 chips.
The dock desigen scheme is: VL171+TUSB8041(x2)+CS5261+SR900AI.
The TYPE-C female interface is used. The USB3.0 interface uses the TYPE-A female interface
VL171 is a type-c interface bidirectional commutator chip
TUSB8041 is the USB3.0 HUB chip, and two chips are cascelled. Chip A uses 3 downstream USB3.0 ports and the other 1 downstream USB3.0 port is connect to the upstream port of chip B. Chip B uses only 1 downstream USB2.0 ports to connect to the USB to network port chip SR900AI.
The CS5261 is a 2-wire DP to HDMI chip. (HDMI function is displayed normally)
The SR900AI is a USB2.0 to network conversion chip (not work yet).
The current situation is that the computer can recognize 2 superspeed USB hubs. (as picture) However, all 4 TYPE-A USB interface can not be used, the computer does not recognize any USB flash drive or other usb devices. Attached pdf file is the dock schematic, please help to me to find out where is incorrect。 Thanks