This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDES960: I2C and INTB pull-up voltage

Genius 17555 points
Part Number: TDES960


Hello,

 

My customer wants to use INTB with 3.3V pull-up and I2C with 1.8V pull-up.

The datasheet recommends to set the IO voltage at I2C voltage which is 1.8V.

If IO voltage is set at 1.8V, is it acceptable to put 3.3V pull-up on INTB pin?

 

Regards,

Satoshi Obata