Part Number: SN65HVD78
Hi Expert,
Is it possible to combine D and R pin together for half-duplex RS-485 application as below configuration?
The left side of SN65HVD78 is FPGA HR Bank, it is Bi-direction pin.

Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD78
Hi Expert,
Is it possible to combine D and R pin together for half-duplex RS-485 application as below configuration?
The left side of SN65HVD78 is FPGA HR Bank, it is Bi-direction pin.

Thanks.
In the configuration shown, the D and R pins are separate. Only the DE and /RE pins are combined.
Connecting D and R together is possible, as long as you ensure that the direction control signal (DE/RE) is correct.
Hi Ryan,
The diagram shows the enables tied together - not the R and D pins - so please see below for an answer to both configurations:
1. The enables can be shorted together so that the combination of the pins acts as a single direction control pin. That is fine and very common use case.
2. R and D can be shorted together - but only the receiver or driver should be active at one time - so essentially if you were to short R and D together you would also need to short /RE and DE together to ensure that the receiver and driver are never active at the same time or else you are just creating a feedback loop where the R pin will drive the D pin which will drive the A/B pins which will go back to the R pin making communication impossible.
If you have any other questions please let me know.
Best,
Parker Dodson